MPC5674F addressable memory with 16-bit bus is only 64KB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5674F addressable memory with 16-bit bus is only 64KB?

Jump to solution
1,562 Views
gabrielmarques
Contributor I

Hello,

I'm working on a new design where we use the MPC5674F EBI to connect an FPGA in 16-bit muxed data/addr mode (D_ADDR_16_31 routed to FPGA).

The FPGA behaves just like a SRAM from the cpu point of view, and we have an assembled prototype already.

Reading trough the datasheet, ref. manual or the External_Bus_Interface_FAQs_draftC.pdf documents didn't clarified this to me.

UserMan section "29.4.2.7 Size, Alignment and Packaging on Transfers" states: 

• 16-bit access, address bit 31 must be 0, and

The EBI never generates a misaligned external access

Our expectation is that we could map 64Kaddr (128Kbytes) on the FPGA, but our current tests show that we cannot access odd addresses on the EBI.

 

Is that a real limitation of this microcontroller or am I doing something wrong?

Labels (1)
1 Solution
1,313 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Your schematic does not help me too much as I don’t see there how these lines are processes by FPGA. Expected usage of multiplexed addresss/data but is using of external address latch, what’s in your case is apparently managed by FPGA itself.

 

pastedImage_3.png

The example you have pointed out assumes standard memory connection as described in section 4 of mentioned document.

It means ADD31 is unconnected and its functionality is basically replaced by WE0 and WE1 lines, the same way I would expect FPGA would be connected to EBI module.

 

Your address mask is 0xFFFF8000 =

0b1111_1111_1111_1111_1000_0000_0000_0000

 

Final address will be

0b0011_0000_0000_0000_0xxx_xxxx_xxxx_xxxx

 

Number of xs there is 15 thus address range 2^15=32kByte

 

You have 16-bit port. It means ADD31 is not connected.

0b0011_0000_0000_0000_0XXX_XXXX_XXXX_XXXx

 

Let’s say you have 8-bit write on address 0x30000000

In address phase, all X address lines will be cleared and WE0 line will be asserted.

If you have 8-bit write on address 0x30000001

in address phase, all X address lines will be cleared and and WE1 line will be asserted.

View solution in original post

0 Kudos
Reply
6 Replies
1,313 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I think I have just shown you are configuring for 32kByte. And also how it addresses even/odd bytes over 16-bit bus.

If you set address mask as s 0xFFFF0000 you will have 64kBytes

0 Kudos
Reply
1,313 Views
marceloteiderlo
Contributor I

Yes, but even if I change address mask to 0xFFFE0000, I can't address 128kBytes (64k 16-bit words), right? I'm limited to 64kBytes, because I can't use ADD31. Is there a way to configure a 16-bit data bus (even if it requires the EBI to be connected differently) to address by word, or is my only option to use a 32-bit data bus?

0 Kudos
Reply
1,313 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I don’t understand you too much. Yes, 29.4.2.7 says what you mentioned but it says following

„Natural alignment for the EBI means:

  • Byte access can have any address
  • 16-bit access, address bit 31 must be 0
  • 32-bit access, address bits 30-31 must be 0
  • For burst accesses of any size, address bits 29-31 must be 0”

 

and

 

“Even though misaligned non-burst transfers from internal masters are supported, the EBI naturally aligns the accesses when it sends them out to the external bus, splitting them into multiple aligned accesses if necessary.“

 

Yes, you can address the whole 128kByte range.

Could you show me your scheme of connection and your EBI setup? Also tell me details about the issue.

0 Kudos
Reply
1,313 Views
marceloteiderlo
Contributor I

Hello,

I work on the same project as gabrielmarques‌, and I was assigned to this task.

The following excerpts of our schematics show the EBI connections with the FPGA (Chip Select 1 is used with the FPGA):

FPDL_a.PNG

The pins used are configured according to the following table:

PCR No.Pin AssignmentFunctionValue
256PrimaryD_CS00x443
257Alternate 1D_ADD_DAT310x843
258Alternate 1D_TEA0x843
259-265PrimaryD_ADD[12:15]0x443
263-277Alternate 1D_ADD_DAT[16:30]0x843
278-293PrimaryD_ADD[16:30]0x443
294-304PrimaryD_RD_RW, D_WE0, D_WE1, D_OE, D_TS, D_ALE, D_TA, D_CS1, D_BDIP, D_WE2, D_WE30x443
305-307PrimaryD_ADD[9:11]0x443

EBI registers are configured with the following:

EBI_MCR = 0x804
EBI_CAL_BR1 = 0x300008A7
EBICALOR1 = 0xFFFF8000

On External_Bus_Interface_FAQs_draftC.pdf document, it is stated:

Internal address lines are assigned to external address lines the same way and in the same order. Considering you have set CS for whole EBI space in binary
0b001x_xxxx_xxxx_xxxx_ xxxx_xxxx_xxxx_xxxx_xxxx_xxxx
'x' here are mentioned bits 3-31
For instance, considering the device offers 22 address lines and non-multiplexed mode has been choosen, bits 9-30 will be reflected on the external bus D_ADD [9:30] ('X'):
0b001x_xxxx_xXXX_XXXX_XXXX_XXXX_XXXX_XXXx
There is 22 address line thus maximum memory size is 8Mbytes (=2^23 because of 16-bit data bus and so D_ADD31 is not used) per chip select.

This indicates that, on the above example, you can address 2^23 bytes, but only 2^22 addresses. On our example, using a 16-bit data bus, we can address 64Kbytes, but only 32K addresses. Is that correct?

0 Kudos
Reply
1,314 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Your schematic does not help me too much as I don’t see there how these lines are processes by FPGA. Expected usage of multiplexed addresss/data but is using of external address latch, what’s in your case is apparently managed by FPGA itself.

 

pastedImage_3.png

The example you have pointed out assumes standard memory connection as described in section 4 of mentioned document.

It means ADD31 is unconnected and its functionality is basically replaced by WE0 and WE1 lines, the same way I would expect FPGA would be connected to EBI module.

 

Your address mask is 0xFFFF8000 =

0b1111_1111_1111_1111_1000_0000_0000_0000

 

Final address will be

0b0011_0000_0000_0000_0xxx_xxxx_xxxx_xxxx

 

Number of xs there is 15 thus address range 2^15=32kByte

 

You have 16-bit port. It means ADD31 is not connected.

0b0011_0000_0000_0000_0XXX_XXXX_XXXX_XXXx

 

Let’s say you have 8-bit write on address 0x30000000

In address phase, all X address lines will be cleared and WE0 line will be asserted.

If you have 8-bit write on address 0x30000001

in address phase, all X address lines will be cleared and and WE1 line will be asserted.

0 Kudos
Reply
1,313 Views
marceloteiderlo
Contributor I

Back to the original question, using a 16-bit muxed data/addr, is it possible to address 64kWords (i.e.: 128kBytes) or I'm limited to 64kBytes (i.e.: 32kWords)?

0 Kudos
Reply