MPC5674F EMIOS CBDR Value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5674F EMIOS CBDR Value

ソリューションへジャンプ
394件の閲覧回数
erdincnamal
Contributor II

Hi,

I tried to assign "0" decimal value to EMIOS' CBDR register. After I set the value to 0 (without resetting), in my next duty-frequency change attempts, when I tried a value that would give 50% duty (CADR = 500, CBDR = 1000), I saw that I could not produce PWM. This problem continued until I reset it. 

My question is, do I need to do such a range check and is the reference available in the manual or in a different document? Unfortunately, most links related to EMIOS in the forum are broken. I would be happy if you help.

Best regards,

Erdinc

タグ(3)
0 件の賞賛
返信
1 解決策
369件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi

you did not mention mode used. So refer to chapter 22.4.1.1 Unified Channel Modes of Operation of the device Reference Manual for mode description and explanation for CARD/CBDR register values and usage for each modes. 

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
364件の閲覧回数
erdincnamal
Contributor II

Thanks I found

0 件の賞賛
返信
370件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi

you did not mention mode used. So refer to chapter 22.4.1.1 Unified Channel Modes of Operation of the device Reference Manual for mode description and explanation for CARD/CBDR register values and usage for each modes. 

BR, Petr

0 件の賞賛
返信
367件の閲覧回数
erdincnamal
Contributor II
I use in mode 101_1010 OPWFMB Output Pulse Width and Frequency Modulation Buffered, (flag on A or B matches)
0 件の賞賛
返信