Hi,
I tried to assign "0" decimal value to EMIOS' CBDR register. After I set the value to 0 (without resetting), in my next duty-frequency change attempts, when I tried a value that would give 50% duty (CADR = 500, CBDR = 1000), I saw that I could not produce PWM. This problem continued until I reset it.
My question is, do I need to do such a range check and is the reference available in the manual or in a different document? Unfortunately, most links related to EMIOS in the forum are broken. I would be happy if you help.
Best regards,
Erdinc
解決済! 解決策の投稿を見る。
Hi
you did not mention mode used. So refer to chapter 22.4.1.1 Unified Channel Modes of Operation of the device Reference Manual for mode description and explanation for CARD/CBDR register values and usage for each modes.
BR, Petr
Thanks I found
Hi
you did not mention mode used. So refer to chapter 22.4.1.1 Unified Channel Modes of Operation of the device Reference Manual for mode description and explanation for CARD/CBDR register values and usage for each modes.
BR, Petr