MPC5668G DSPI_C only accessible by Core z0; maybe depends on AIPS/AXBS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5668G DSPI_C only accessible by Core z0; maybe depends on AIPS/AXBS?

769件の閲覧回数
tanzou_mechmet
Contributor I

Hello everybody,

at first of all, I'm sorry because of my not very good English!

I'm working on the MPC5668G which has two Cores z0 and z6. I have to use the DSPI module and I can only use the DSPI_C interface. Until now I was using only the z6 Core and while I wanted to implement the code for DSPI_C, I got a DTLB (Data Translation Lookaside Buffer) error on the debugger.

I have tested the other DSPI interfaces (DSPI_A, DSPI_B, DSPI_D) and the other Core z0 and I could determine, that

the Core z6 can successfully access only the DSPI_A and DSPI_B interfaces,

while

the Core z0 can successfully access only the DSPI_C and DSPI_D interfaces.

I have looked up to into the Reference Manual (RM) and I have seen one difference:

DSPI_A and DSPI_B are within the memory region AIPS_B (AXBS Port S7)

while

DSPI_C and DSPI_B are within the memory region AIPS_A (AXBS Port S6)

So, I think, that the AIPS_A is only accessible by Core z0 and the AIPS_B is only accessible by Core z6. But in the RM I can't see this information. So could you please explain me, if I am right or if it is possible to change configurations?

2 返答(返信)

557件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, not really. It can be accessed by e200z6 core as well but is is needed to define MMU region for AIPS_A space,

We have been using following MMU setting in Lauterbach:

;MMUSCR0: enable address translation bypass

Data.Set SPR:0x3F4 %LONG 0x80000000

;set up TLBs

MMU.TLB1.SET 0. 0xC0000500 0xFFF0002A 0xFFF0003F ;peripherals and boot rom

MMU.TLB1.SET 1. 0xC0000900 0x00000020 0x0000003F ;FLASH

MMU.TLB1.SET 2. 0xC0000900 0x20000020 0x2000003F ;external SRAM

MMU.TLB1.SET 3. 0xC0000500 0x40000028 0x4000003F ;internal SRAM

MMU.TLB1.SET 4. 0xC0000500 0xC3F00008 0xC3F0003F ;AIPS_A

 

In Codewarrior it is configured in INIT_Derivative function.

 

AIPS_A must be initialized:

 

/* Write one MMU Table Entry:               */

/* r3, r4, r5 and r6 must hold              */

/* the values of MAS0, MAS1, MAS2 and MAS3  */

asm void InitAIPS_A( void )

{

    nofralloc

 

    mflr     r29                         /* Save off return address in NV reg */

   

    // MMU.TLB1.SET 4. 0xC0000500 0xC3F00008 0xC3F0003F ;AIPS_A

   

    #define MAS0_AIPS_A 0x10040000

    #define MAS1_AIPS_A 0xC0000500

    #define MAS2_AIPS_A 0xC3F00008

    #define MAS3_AIPS_A 0xC3F0003F

    e_lis   r3, MAS0_AIPS_A@h

    e_or2i  r3, MAS0_AIPS_A@l   

    e_lis   r4, MAS1_AIPS_A@h

    e_or2i  r4, MAS1_AIPS_A@l   

    e_lis   r5, MAS2_AIPS_A@h

    e_or2i  r5, MAS2_AIPS_A@l

    e_lis   r6, MAS3_AIPS_A@h

    e_or2i  r6, MAS3_AIPS_A@l       

    msync

    se_isync        

    bl  WriteMMUTableEntry

    se_isync

 

    mtlr    r29

 

    blr

}

557件の閲覧回数
tanzou_mechmet
Contributor I

Thanks a lot davidtosenovjan‌. Your code is working. For other people, that are using GCC and not CodeWarrior like me, here is my code with GCC-specific syntax for asm code:

__asm __volatile(
        //MAS0_AIPS_A Konfiguration:    0x10040000
        //MAS1_AIPS_A Konfiguration:    0xC0000500
        //MAS2_AIPS_A Konfiguration:    0xC3F00008
        //MAS3_AIPS_A Konfiguration:    0xC3F0003F

        "mflr %r29; \
        e_lis %r3, 0x10040000@h; \
        e_or2i  %r3, 0x10040000@l; \
        e_lis   %r4, 0xC0000500@h; \
        e_or2i  %r4, 0xC0000500@l; \
        e_lis   %r5, 0xC3F00008@h; \
        e_or2i  %r5, 0xC3F00008@l; \
        e_lis   %r6, 0xC3F0003F@h; \
        e_or2i  %r6, 0xC3F0003F@l; \
        msync; \
        se_isync;"

        /*        se_bl  WriteMMUTableEntry; \*/
        /* Write MMU Assist Register 0 (MAS0); SPR 624 */
        "mtspr   624, %r3;"
        /* Write MMU Assist Register 1 (MAS1); SPR 625 */
        "mtspr   625, %r4;"
        /* Write MMU Assist Register 2 (MAS2); SPR 626 */
        "mtspr   626, %r5;"
        /* Write MMU Assist Register 3 (MAS3); SPR 627 */
        "mtspr   627, %r6;"
        /* Write the table entry */
        "tlbwe;"

        "se_isync; \
        mtlr %r29;"
    );

0 件の賞賛