MPC5645S ko with external oscillator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5645S ko with external oscillator

381 次查看
PCC
Contributor I

Hello,

 

The cpu runs correctly with 16MHz internal RC   , and runs correctly with an 8Mhz QUARTZ,

But when connecting an  External oscillator 8MHZ MASTERCRISTAL MCS01Y-B-8MHZ  level  1,2V , square wave 

=> the cpu doesnt start correctly because it detects 

S_FXOSC =0 (0 fast external crystal oscillator (4-16 MHz) is not stable)

 

the oscillator is  MASTERCRISTAL MCS01Y-B-8MHZ  level is 1,2V , square wave is clean , stable and accurate 8MHZ

The trace of EXTAL is short (3.5mm) , the XTAL is left unconnected (we try too with EXTAL grounded )

 

With 3 différents boards , the problem is the same 

 

Seems to be a soft initialization problem

Can any body help us ?

Thanks for all

 

Pierre CAZENAVE

0 项奖励
0 回复数