MPC5644A Reading ADC Values With Different Crystals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5644A Reading ADC Values With Different Crystals

647 Views
bulent_kupeli
Contributor II

Hello, I am using MPC5644A microcontroller with 20 MHz and 40 MHz crystals. When I used 20 MHz with the MPC5644A, I read the some values ​​from the ADC channel but when I use the 40 MHz crystal with same code, I cannot read any value from the ADC channels, I checked my power and ADC signals and did not see any problems. I checked the pins of the MPC5644A but did not see any issues, do you know why I am seeing this problem? Can you help me ?

Thank you,

Bülent

Tags (2)
0 Kudos
1 Reply

600 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

This is the same thread as following one:

https://community.nxp.com/t5/MPC5xxx/MPC5644A-ADC/m-p/1201028/highlight/false#M16881

Please continue with that one. Thanks

0 Kudos