MPC5643L_some details about CTU FIFO and DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5643L_some details about CTU FIFO and DMA

Jump to solution
2,477 Views
yanna
Contributor IV

About CTU FIFO

 

Q1: I want to use CTU trigger send a command to ADC, then use FIFO 0 overflow event trigger a DMA transfer. I feel unsure about the FIFO 0 threthold value. For example:

IF FIFO 0 threthold equals 4, how many ATD results when FIFO 0 contains will cause a DMA transfer, 4 or 5 ?

 

 

Q2: I cann’t quite understand the FIFO control register,for example: FIFO 0 overflow interrupt enable bit .

148622_148622.pngCTU_FIFO0.png

From the corresponding codes of MPC5643L technical support (PWM triggered measurement concept) written by Peter Vina and AN4797 by Yves Briant ,we get know that they both use FIFO 0 overflow event trigger a DMA transfer. What’s the relationship between the event and FIFO 0 overflow interrupt enable bit which they both set?

 

Following code is from the technical support by Peter Vina.

 

CTU.TH1.B.THRESHOLD0 = 0xE;   /* FIFO 0 Threshold. Maximum value of 15, as the threshold value must be less than the

                       number of FIFO 0 entries. */

CTU.FCR.B.FIFO_OVERFLOW_EN0 = 1;  /* FIFO 0 threshold Overflow interrupt enable - read FIFO 0 in this nterrupt */

 

I think we only need to configure the corresponding DMA enable bit for FIFO 0 bit and DMA channel source, isn’t it right? Why we need to configure   FIFO 0 overflow interrupt enable bit ?

Such as   CTU.FDCR.R  = 0x1; // Enable DMA for FIFO0

                 DMAMUX.CHCONFIG[5].B.SOURCE = 8;   // CTU FIFO0 threshold

 

Thanks very much!

Yanna

Labels (1)
Tags (3)
1 Solution
1,813 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

1. you don't have to enable FIFO interrupt.

2. If you enable DMA transfer then it is done on FIFO threshold.

In my application FIFO depth is 15 (0 to 15), the number of ADC results in FIFO is 16 (this means depth 15 as FIFO starts from FIFO_0).

Peter

View solution in original post

11 Replies
1,813 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

A3:

Each submodule can request a DMA read access for its capture FIFOs and a DMA write request for its double buffered SUBn_VALx registers.

pastedImage_0.png

You completely misunderstood the usage of this feature.

It is desired for update of double buffered VALx registers. For example is you wan to generate continuous duty cycle increase from 0% to 100%. The DMA transfer is triggered when Reload flag is set!

Make sure you read the reference manual before asking a questions. All these information are there.

If you require training on MPC5643L peripheries do not hesitate to order one.

A4: Configure your DMA to do so, if you want to avoid CPU intervention. No special sample code is needed, just configure DMA to transfer bytes you want to.

A5: Yes SW interrupts are drawing you computational power of CPU. Also a time critical motor control applications benefits from CTU/DMA.

CTU is there to support accurate and fast measurements for high speed motor applications. But all this is in reference manual!

pastedImage_4.png

Peter

0 Kudos
1,814 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

1. you don't have to enable FIFO interrupt.

2. If you enable DMA transfer then it is done on FIFO threshold.

In my application FIFO depth is 15 (0 to 15), the number of ADC results in FIFO is 16 (this means depth 15 as FIFO starts from FIFO_0).

Peter

1,813 Views
yanna
Contributor IV

Q5: Hi,Peter.

I think you may only want to explain how to use FlexPWM and CTU and eDMA module in your application.

In practical application,did a FIFO DMA transfer without CPU intervention have a great advantage

over a FIFO interrupt with CPU intervention ?

For example:

In your application,you transfer the data with a DMA request.

Also it can use FIFO 0 interrupt event to tranfer data,such as FIFO 0 overflow interrupt

First,enable the FIFO 0 interrupt

(CTU.FCR.B.FIFO_OVERFLOW_EN0 = 1; /* FIFO 0 threshold Overflow interrupt enable

Second,write the FIFO_0 overflow isr code

void  FIFO_0 overflow isr(void)

{

ADC_results[0]= CTU.FRA[0].R   // or ADC_results[0]=ADC.CDRx.R

}

Did transfering the data from FIFO 0 to ADC_results[0] through FIFO 0 interrupt cost much time? How long it will cost? (CTU.FRA[0].R contains 16 bit data )  

I think a DMA transfer have a great advantage when the transfer data was array which contains many data.

Thanks very much!

Yanna

0 Kudos
1,813 Views
yanna
Contributor IV

About FIFO DMA request and FIFO interrupt

Q4:  Hi,peter

       In your application,the data was transferred from CTU FIFO 0 to the address &ADC_results[0] .

pastedImage_0.png

      We know the value in the FIFO 0 not only include the data we need but also the information about the ADC

      unit and channel.

  pastedImage_1.png

    We often get the data using the sentence like temp=ADC_results &&0FFF.

    Did  there exist another method to get the result only include the data(no ADC unit and channel information)

    from the source address? Did there exist sample codes?

   Thanks very much!

   Yanna

0 Kudos
1,813 Views
yanna
Contributor IV

Hi,Peter

Thanks very much! I have got it.

could you help me for another two question above?

Thanks very much!

Yanna

0 Kudos
1,813 Views
yanna
Contributor IV

About DMA_MUX source   comp_val source

Q3:If I want to use FlexPWM0_sub0 valx write DMA request,then I need to configure corresspoding register, like

FLEXPWM_0.SUB[0].DMAEN.B.VALDE = 1;         //Enable DMA

      DMAMUX.CHCONFIG[1].B.SOURCE = 12;   //FlexPWM write request

pastedImage_4.png

so when the counter reach the value of VALx(x=0,1,2,3,4,5),a DMA transfer will occur,is it right?

Is it possible a DMA transfer occur only when the counter reach the value of VAL0  not included other VALx(x=0,2,3,4,5)?  Did there exist the register which select the VALx write request to the comp_val signal?

Thanks very much!

Yanna

0 Kudos
1,813 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I recommend you to have a look on my application example:

MPC5643L PWM_ADC measurement concept

Peter

0 Kudos
1,813 Views
yanna
Contributor IV

HiPeter

My understanding is the FIFO interrupt enable bit needn’t be configured when we need use FIFO DMA request event.

  1.  Your applitation configure FIFO interrupt enable bit directly without explaination.

   We read FIFO through a DMA transfer, not interrupt.

pastedImage_17.png

  2.  Your applitation set FIFO threthold for 0XE, my understanding is when FIFO contains 16 ATD results ,

       a DMA transfer will occur.But in your applitation,you said FIFO reached depth of 15, I think it should be 16.

       is my understanding wrong?

  3.  Only question 1 and 2 have relation with your applitation, the other two haven’t.

Thanks very much!

Yanna

0 Kudos
1,813 Views
yanna
Contributor IV

About DMASERQ register

First,I want to verify whether my understanding about the channel service request is right.

Channel service requests include hardware service request and software request and channel linking request.

hardware service request is from DMA peripheral sources ,

software request is determined by TCD.start bit,

if we use a channel’s hardware service request,we should configure correspoding DMA_MUX channel source and enable request bit(DMAERQL or DMASERQ). However ,if we use software request and channel linking request,we needn’t to configure corresponding enable bit, is it right?

I think there may exist typos in page 408 of RM.

Thanks very much!

Yanna

0 Kudos
1,813 Views
petervlna
NXP TechSupport
NXP TechSupport

1.Right. See my drawing.

pastedImage_0.png

If you use SW request you needn't to configure DMA mux. In case of HW request you must configure DMA MUX.

2. There is no typo in RM. But the description is little confusing. I hope that following picture will bring the light to the problematic.

pastedImage_1.png

Peter

1,813 Views
yanna
Contributor IV

HiPeter.

Thanks very much! Your explanation is very clear .

Table 19-7 describes the structure of DMASERQ[SERQ] field, not DMASERQ.

I’m sorry for my carelessness.

Looking forward to your reply about question3&4&5(Q3&Q4&Q5) below.

Thanks very much!

Yanna

0 Kudos