MPC5634芯片发热

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5634芯片发热

1,665 Views
liujian
Contributor I

我参考网站上的MPC5634的设计 设计一个电路,发现MPC5634烫手,请问该如何解决,但是将PIn13引脚的对地电容22uf 和0.1uf  取下后芯片便不再发热,请问这个两个电容能否不焊接,但是不焊接时发现此管脚的电压波形为锯齿波附件是我的电路图,请指教!!

105114_105114.pngpastedImage_0.png

Labels (1)
0 Kudos
6 Replies

1,131 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The VRC33 capacitors have to be used to bypass internal regulator.

Seems those are wrong. Have you measured the VRC33 when capacitors are placed?

Try to use different one.

BR, Petr

0 Kudos

1,131 Views
liujian
Contributor I

I change a few capacitance values are not the same tantalum capacitor, the voltage is 3.4 v,When I don't meet capacitor, the voltage is 4 v, but is the sawtooth waveform。

0 Kudos

1,131 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Can I recommend you to post your question in English ?

Google Traduction:

Design Design MPC5634 my reference site on one circuit and found MPC5634 hot, how to fix it, but will PIn13 pin capacitance to ground 22uf and 0.1uf remove heat after the chip will no longer ask whether the two capacitors no welding, but when not welding found this pin voltage waveform sawtooth attachment is my schematic, please advise!

I moved the Question to hardware team.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,131 Views
liujian
Contributor I

The translation above is my problem,Please help to solve!

thanks

0 Kudos

1,131 Views
xingchaofu
Contributor I

你好:

   你使用的是什么封装的芯片?确定pin13引脚是电源引脚吗?多少pin的?仔细核实下数据手册引脚定义

0 Kudos

1,131 Views
liujian
Contributor I

我使用的是176引脚的,13pin 不是电源引脚,那是网络标号,该引脚没有供电电源,而是对外提供电源。给下载口的上拉电阻提供电源

0 Kudos