MPC5604S - Flash library issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5604S - Flash library issue

557 次查看
akhilprasad
Contributor III
I am using MPC5604S controller and the self-programming flash library provided from NXP. I have a requirement to write certain numbers to a particular memory location using the flash write operation. But one constrain is that i need to refresh the controller in every 10ms else the controller will reset or go to sleep. So i am refreshing watchdog inside the callback routine. 
But the issue I am facing is that when I am trying to write the number to the controller using flash library,the controller is resetting. That means watchdog refreshing is not happening.
Kindly provide your suggestions ASAP.
0 项奖励
1 回复

467 次查看
akhilprasad
Contributor III

Now this resetting issue is happening only when I am trying to write the number through CAN to the board and the board is stand alone i.e without connecting debugger.

0 项奖励