Hello,
I want to create a bootloader. This question is for the application.
I want to move my application to address 0x8000.
I'm the meaning I have changed all addresses.
But in case of:
GROUP : {
.text : {}
.text_vle (VLECODE) ALIGN(0x08) : {
*(.text)
*(.text_vle)
}
.rodata (CONST) : {
*(.rdata)
*(.rodata)
}
...
} > internal_flash
the section .text_vle have different load and run addresses.
Memory map: Starting Size File ROM RAM Buffer S-Record address Offset Address Address Line | |
.text_vle 0000a000 000074e0 000008c0 00002000 00002000 | 2 |
objdump confirm, that this section is located on 0x2000 within the .elf file
In case I change the Load address for .text_vle the next section .rodata is move to 0x2000.
What is wrong?
Where is the address 0x2000 from?
I attached my Linker file and my Mapping file.
In general:
I'm the meaning, that the Linkerfile definition
GROUP : {
...
.rodata (CONST) : {
*(.rdata)
*(.rodata)
}
...
} > internal_flash
means, that load and run address is the same and it is located in "internal_flash"-Memory.
Thank you.
Original Attachment has been moved to: MPC5604P_M26V_BOOT.lcf.zip
Original Attachment has been moved to: Boot_Slave.MAP.zip
已解决! 转到解答。
Hi,
just quick answer now - take a look at document AN_qorriva_bootloader.pdf in:
https://community.freescale.com/servlet/JiveServlet/download/427962-279359/bootloader.zip
I described all settings that need to be done when moving application to another address.
If it still doesn't work, just let me know.
Regards,
Luks
Hi,
just quick answer now - take a look at document AN_qorriva_bootloader.pdf in:
https://community.freescale.com/servlet/JiveServlet/download/427962-279359/bootloader.zip
I described all settings that need to be done when moving application to another address.
If it still doesn't work, just let me know.
Regards,
Luks
Hello Lukas,
Thank you very much.
Chapter "Building a ROM Image" was the relevant part.
I read the chapters and I understand, that my "normal" used value und your suggest value for the "RAM Buffer address" is located in Flash.
Is this setting not used?
Also I found the description of "At startup, the program uses the _rom_copy_info
structure..." with the hint, that I can also copy code to the RAM automatically.
But I don't found information, where I can control the .PPC.EMB.seginfo/_rom_copy_info functionality.
Are there additional documentation for the Linker internas as in the help document?
Regards
Steffen
Hi Steffen,
I'm not CodeWarrior expert, not sure how it works exactly but the documentation says that the addresses should be set to the same value:
Regarding code in RAM - I have shared sample project in this thread:
or direct link:
Take a look at main.c and linker file. If you do it in this way, the code will be automatically copied to RAM during startup.
Best Regards,
Lukas
Hello Lukas,
thank you very much for your help and your many small examples.
Do you have an addition documentation for Linking internals?
I understand now, that the following two lines are differently
#pragma section RX ".ramfunction" ".ramfunction" data_mode=far_abs code_mode=far_abs
#pragma section code_type ".ramfunction" ".ramfunction" data_mode=far_abs code_mode=far_abs
But I cannot find additional information for the additional work of code_type.
The documentation say only, that I require with the first line additional _declspec() .
---------
Also I search additional infromation to create an true uninitialized section (NOINIT). Means a section that is not erased with zeros at the beginning (like .bss).
#pragma section RW ".xx" ".command"
__declspec(section ".xx") U8 cobl_command[16];
I think I require this information:
(Mapping)
2] __init_data (func,weak) found in Runtime.PPCEABI.VS.UC.a __start.o
3] _bss_init_info (object,global) found in Linker Generated Symbol File
How can I remove my .command section from the _bss_init_info list?
(The alternativ way - remove this region completely and use a pointer to this "unknown" region I know.)
Background:
I want to have a memory region for communication between application and bootloader. The startup code should not erase and initialize it.
Thank you very much.
bye
Steffen
not expert of this cpu, but you should be able to define yourself where the sections are set in memory.
This is what the linker file is needed for. So define section names and assign the addresses you want. Then
you should be able to put them there, using the > symbol.
Hi,
of course I did set the memory definition in the attached Linkerfile.
An I used the section definition as you suggest.
But the linker seems to have an additional "anything", that move sections without addition LOAD() to address 0x2000. I cannot find this setting.
I'm the meaning, that in case od using a linker file all settings located in it.