Hi,
If LOM bit is asserted in Freeze mode, the FlexCAN module enters Listen-Only Mode.
Transmission is disabled, all error counters are frozen and the module operates in a CAN Error Passive mode. Only messages acknowledged by another CAN station will be received. If FlexCAN detects a message that has not been acknowledged, it will flag a BIT0 error, as if it was trying to acknowledge the message. RX interrupts are functional in LOM mode normally.
Attached if simple example I did for TRK-MPC5606B. CAN0 is used to send message, CAN1 to receive it with a help of RXFIFO.
I have added CAN2 to work in LOM mode to receive all standard ID to MB0 and extended IDs to MB1. Interrupt is enabled.
BR, Petr
Hi,Peter:I transplant the 5606B code you offered to MPC5604B and it works well,Buff[9] for Tx and Buff[5] for Rx function with the same CAN0 channel.Then I adjust the Buff[6] to Buff[5],unfortunately,The Rx does not work.
(1)Buff[6] and Buff[5] shares the same interrupt vector ,No.69--Flexcan_Buff_04_07
(2) CAN_0.IMRL.R = 0x00000040; // enable BUF06I interrupt
(3)if(CAN_0.IFRL.B.BUF06I)
{
/* upon receiving the interrupt flag */
/* check the ID field */
/* not really needed in this example */
/* useful in case when multiple IDs are received
* by the FIFO (Rx mask feature) */
temp = CAN_0.BUF[6].ID.R;
//if(( 0x12340000 ) != temp)
//{
/* error ! trap here.
* we have configured this MB to receive
* just ID 0x12340000 and not another */
// while(1) {}
// }
rxlength = (uint8_t) CAN_0.BUF[6].CS.B.LENGTH;
/* read the received data */
for (j=0; j<rxlength; j++)
{
RxDATA[j] = CAN_0.BUF[6].DATA.B[j];
}
u8_rxdata=CAN_0.BUF[6].DATA.B[0];
temp = CAN_0.TIMER.R; /* Read TIMER to unlock message buffers */
//CAN_0.IFRL.R = 0x00000020; /* clear the BUF05I bit - bit 5 */
CAN_0.IFRL.R = 0x00000040;/* clear the BUF06I bit - bit 6 */
}
I am puzzled with it,can you offer me some help?
Thank you Petr Stancik.
Assuming that there are only two nodes. one configured in LOM mode and the other in Normal mode transmitting a periodic message.
since there are no other nodes to ACK the message transmitted by Normal mode, will the node in LOM mode will just flag a BIT0 error or will it flag a BIT0 error as well as receive the message in the configured MB.
I am yet to get my evaluation board to do this. will post again once i have the board.
Thanks for your input.
Hi,Peter:I transplant the 5606B code you offered to MPC5604B and it works well,Buff[9] for Tx and Buff[5] for Rx function with the same CAN0 channel.Then I adjust the Buff[6] to Buff[5],unfortunately,The Rx does not work.
(1)Buff[6] and Buff[5] shares the same interrupt vector ,No.69--Flexcan_Buff_04_07
(2) CAN_0.IMRL.R = 0x00000040; // enable BUF06I interrupt
(3)if(CAN_0.IFRL.B.BUF06I)
{
/* upon receiving the interrupt flag */
/* check the ID field */
/* not really needed in this example */
/* useful in case when multiple IDs are received
* by the FIFO (Rx mask feature) */
temp = CAN_0.BUF[6].ID.R;
//if(( 0x12340000 ) != temp)
//{
/* error ! trap here.
* we have configured this MB to receive
* just ID 0x12340000 and not another */
// while(1) {}
// }
rxlength = (uint8_t) CAN_0.BUF[6].CS.B.LENGTH;
/* read the received data */
for (j=0; j<rxlength; j++)
{
RxDATA[j] = CAN_0.BUF[6].DATA.B[j];
}
u8_rxdata=CAN_0.BUF[6].DATA.B[0];
temp = CAN_0.TIMER.R; /* Read TIMER to unlock message buffers */
//CAN_0.IFRL.R = 0x00000020; /* clear the BUF05I bit - bit 5 */
CAN_0.IFRL.R = 0x00000040;/* clear the BUF06I bit - bit 6 */
}
I am puzzled with it,can you offer me some help?