MPC55xx,FMPLL,Loss-of-clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC55xx,FMPLL,Loss-of-clock

1,361 Views
ypchen
Contributor III

Hello NXP:

MPC55xx,External Reference Mode-- 16MHz , and the system clock is 132MHz.

The other SYNCR's configuration is as follows:

FMPLL_SYNCR[LOCEN]  = 0;

FMPLL_SYNCR[LOLRE]  = 0;

FMPLL_SYNCR[LOCRE]  = 0

If the external  clocks fall below the threshold frequency, what the system will happen ?  stop ,or enter self-clock mode ?

6 Replies

797 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, Regarding loss-of-lock (frequency changes out of specified range) :

pastedImage_1.png

While the FMPLL is in an unlocked condition, the system clocks continue to be sourced from the FMPLL as the FMPLL attempts to re-lock. Consequently, during the re-locking process, the system clock frequency is not well defined and may exceed the maximum system frequency thereby violating the system clock timing specifications. Thus it is potentially dangerous configuration and it is recommended to have enabled reset reaction.

Regarding loss-of-clock (clock dissapears):

pastedImage_2.png

Loss of reference frequency is defined as the reference frequency detected internally, which transitions the PLL into self-clocked mode. Again it is recommended to have enabled reset for this event.

797 Views
ypchen
Contributor III

Hi, 

In the  Reference Manual : 11.4.2.6.1 Alternate/Backup Clock Selection
"If the user enables loss of clock by setting FMPLL.SYNCR[LOCEN] =1, then the FMPLL will transition
system clocks to a backup clock source in the event of a clock failure as per Table 11-9."

My question is:  If Loss-of-clock disabled ( FMPLL.SYNCR[LOCEN] =0),and then the external clock (16MHz) dissapear, the FMPLL will also enter self-clock mode (SCM) ? or what will happen? It seems that the content is not explained in the manual.

0 Kudos

797 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

If FMPLL.SYNCR[LOCEN] =0, than lock-of-clock is not functional thus it does not detect any issue and MCU does not run.

797 Views
ypchen
Contributor III

Hi,David :

External Reference Mode(16MHz),  system clock is 132MHz , and  FMPLL.SYNCR[LOCEN] =0 .

First ,  power-up the board , the MPC5554 run @ 132MHz , and then I disabled the OSC (external clock  dissapear)   , but the  MCU  is still running ,the system clock is lower (~62MHz) .

Why ?

0 Kudos

797 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please clarify, which microcontroller you use?

Regards,

Martin

797 Views
ypchen
Contributor III

hello:

the microcontroller is MPC5554MZP132.

0 Kudos