(MPC5553)How can I configure global variable in flash memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

(MPC5553)How can I configure global variable in flash memory

1,615件の閲覧回数
limheesun
Contributor II

I want to configure global variable in specific flash address(High address 0x00160000:H7 Block).

so I used flash erase and write sequence function with the Manual.

And EPPC Target in Target settings panels, Small Data and Small Data2 -->0

 

So, I can check the variable is configured in address 0x00160000

Now, My question.

 

Only 'Const' can be saved in flash memory? Or  can be delete or not? The flash erase sequence doesn't operate. The variable "test" value can't be modified in flash??

 

How can I modify this value(test) in flash memory?

 

<lcf>

MEMORY

{

    resetvector:        org = 0x00000000,   len = 0x00000008

    init:               org = 0x00000020,   len = 0x00000FE0

    exception_handlers: org = 0x00001000,   len = 0x00001000

    internal_flash:     org = 0x00002000,   len = 0x00160000

 

    my_Flash:   org = 0x00160000, len = 0x0001E000

 

    internal_ram:       org = 0x40000000,   len = 0x0000A000

    heap  :             org = 0x4000A000,   len = 0x00002000 /* Heap start location */

    stack :             org = 0x4000C000,   len = 0x00004000 /* Start location for Stack */

}

.

.

SECTIONS
{
    .__bam_bootarea LOAD (0x00000000): {} > resetvector

    GROUP : {
      .init LOAD (0x00000020) : {}
      .init_vle (VLECODE) LOAD (_e_init) : {
        *(.init)
        *(.init_vle)
      }
    } > init

    .__exception_handlers  LOAD (0x00001000): {} > exception_handlers

    GROUP  : {
        .text : {}
        .text_vle (VLECODE) ALIGN(0x1000): {
             *(.text)
             *(.text_vle)
         }
        .rodata (CONST) : {
            *(.rdata)
            *(.rodata)
        }
        .ctors : {}
        .dtors : {}
        extab : {}
        extabindex : {}
    } > internal_flash
   
    .__my_Flash LOAD(0x00160000):{}>my_Flash

    GROUP : {
       .__uninitialized_intc_handlertable ALIGN(0x10) : {}
       .data   : {}
       .sdata  : {}
       .sbss   : {}
       .sdata2 : {}
       .sbss2  : {}
       .bss    : {}
    } > internal_ram
}

 

<.c file>

#pragma push

#pragma section all_types ".__my_Flash" ".__my_Flash"

uint32_t test=0x1000;

#pragma pop

 

<write sequence>

 

unsigned int* b = (unsigned int*)address;

 

FLASH.MCR.B.PGM = 1;

 

test = data;

add=&test;

FLASH.MCR.B.EHV = 1;

while(FLASH.MCR.B.DONE == 1){};

FLASH.MCR.B.EHV = 0;
 
FLASH.MCR.B.PGM = 0;

 

 

<Result>

&test = 0x00160000

*test = 0x1000

 

But I can't modify this variable's value.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,377件の閲覧回数
limheesun
Contributor II

Thank you for your help and I checked the code of your example.

I think, I don't understand yet. T.T

I have a global variable, 'Offset'. This variable is modified at once( when the main application is start) by auto calibration function.

So, The auto calibration function will find the 'Offset' value, then I need to save this value in flash address.

And then, after the value save in flash address, I will use this value(Offset) on the main application's operation without the auto calibration even after Power Reset.

So, I used #pragma to configure the variable direct in flash address.

This way has a problem the only constant value can save in flash.

And, I made the flash routine, but there're bus error.

#pragma push

#pragma section all_types ".__my_Flash" ".__my_Flash"

static const vuint32_t WVar=0xAAAAAAAA;

#pragma pop

I want make operation like 'WVar=Offset'.

void Program_FLASH(void)
{
    #define FLASH_HLR_PASSWORD      0xB2B22222

    /* enable high address space */
    FLASH.HLR.R = FLASH_HLR_PASSWORD; // unlock register
    FLASH.HLR.B.HBLOCK = 0x00000000;         // unlock all high blocks

    /* step1. erase H1 (0xC0000-0xFFFFF) */
    FLASH.MCR.B.ERS = 1;
    FLASH.HSR.B.HBSEL = 0x00000001;           // select H1 block
    *((unsigned int*) p_test) = 0xFFFFFFFF;  // interlock write
    FLASH.MCR.B.EHV = 1;                    // start the erase operation
    while(FLASH.MCR.B.DONE == 0){};         // wait for DONE
    FLASH.MCR.B.EHV = 0;
    FLASH.MCR.B.ERS = 0;

    /* step2. program data */
    FLASH.MCR.B.PGM = 1;             
*((unsigned int*)p_test) = Offset; //Is this valid?? This is my main question
//    *((unsigned int*) p_test++) = data_to_be_written[0]; // first write
//    *((unsigned int*) p_test++) = data_to_be_written[1]; // additional write
//    *((unsigned int*) p_test++) = data_to_be_written[2]; // additional write
//    *((unsigned int*) p_test) = data_to_be_written[3];   // additional write
    FLASH.MCR.B.EHV = 1;                                //start the erase operation
    while(FLASH.MCR.B.DONE == 0){}; //wait for DONE
    FLASH.MCR.B.EHV = 0;
    FLASH.MCR.B.PGM = 0;
}

Flash permission only constant like 0x0001?

And I adjust yout example on my code, but there're bus error too.

What I miss? T.T

I hope your help, please and thank you.

0 件の賞賛
返信

1,377件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is typical to define non-volatile data as const storage class.

I have recently shared example code for MPC5643L simple flash programming. It could help you to understand the procedure (although it is different device, principle is the same):

https://community.freescale.com/docs/DOC-101849

Pay attention to main.c file and MPC5643L_my_sections.lcf linker command file.

Hope it helps.

0 件の賞賛
返信