MPC5125 Replace DDR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5125 Replace DDR

跳至解决方案
1,368 次查看
zhangbin_eos
Contributor III

I want to replace the DDR of mpc5125 from 256MB to 512MB,
The hardware has replaced 512MB DDR, which is pin compatible. Without modifying the code, the kernel can start normally, but the DDR displayed is 256MB,
What parts do I need to change to enable the kernel to apply larger DDR?
Do you have any relevant documents or examples for reference?

标记 (2)
0 项奖励
1 解答
1,342 次查看
Pavel
NXP Employee
NXP Employee

Change DDR setting in u-boot configuration file and rebuild u-boot. Find .h file for the MPC5125 board using the following path in u-boot source folder:

/include/config

 

Attached file contains this file for the ads5125 board.

在原帖中查看解决方案

0 项奖励
1 回复
1,343 次查看
Pavel
NXP Employee
NXP Employee

Change DDR setting in u-boot configuration file and rebuild u-boot. Find .h file for the MPC5125 board using the following path in u-boot source folder:

/include/config

 

Attached file contains this file for the ads5125 board.

0 项奖励