MPC 5777C ADC and DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC 5777C ADC and DMA

1,210 Views
nizhang
Contributor II

I have a question regards to the MCAL configuration for DMA and ADC. 

I configured a ADC group under EQADC-A ADC0, when I configure to use FIFO 0 and DMA (For DMA I configured DMA channel and callback function in the MCL module and add interrupt for DMA), it is working properly. However, when I change from FIFO 0 to FIFO 1 and apply similar configurations in the MCL module and interrupt vector table, The ADC is not triggered even through I choose the same trigger source as the one I tested when using FIFO 0. 

Is there any clue that I can fix this problem? 

Thanks a lot 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

948 Views
leonggz
Contributor I

did you change the dma channel used to associate with the corresponding fifo? see dma mapping table 4-5 in the RM. and what is MCL module?

0 Kudos
Reply

948 Views
nizhang
Contributor II

Hello. the MCL module is a Microcontroller library that can configure the DMA channels.

Currently I fixed the issue I listed above. Thanks for the clue.

However, I have a new problem regards to the :  Is it OK to configure two groups that use different FIFOs inside the same ADC hardware unit. And each group use different Hardware trigger sources.

Example:

In ADC unit 0:

Group 1 has channel 1, use FIFO 1 and hardware triggered by ETRIG1.

Group 0 has channel 0, use FIFO 0 and hardware triggered by ETRIG0.  I configured two signals with the phase shift to feed the ETRIG0 and ETRIG1.

Problem: only group 0 is triggered, group 1 has never been triggered.

Is there any way that I can deal with this problem?

Thanks for the help

0 Kudos
Reply