Is there Parallel port for MPC5675K except EBI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there Parallel port for MPC5675K except EBI?

1,055 Views
博张
Contributor I

I want to use parallel port. Is there Parallel port for MPC5675K?  What is the module ?

Labels (1)
0 Kudos
Reply
6 Replies

937 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

what kind of parallel port do you mean? What device do you want to connect? There's EBI, PDI, DRAM controller...

Lukas

0 Kudos
Reply

937 Views
博张
Contributor I

Hi,Lukas:

We want to communicate with external DA without clock signal and address bus.(so we can not use PDI, is it right ?) And we also want to communicate with a Spin decoding chip that using 12 pins to show a data with 12 bits.There is also no clock signal and address bus. There is only an inhibit signal except the 12 bits data signal outputting by 12 pins. So what kind of parallel port can I use with MPC5675K.

And if I use EBI, the rest of the EBI pins can be used as other function ?

Thank you for your attention.I am looking forward to your reply.

Jilin university

zhang.bo

0 Kudos
Reply

937 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

pastedImage_0.png

pastedImage_1.png

0 Kudos
Reply

937 Views
博张
Contributor I

Hi,lukas:

Thank you very much for your reply.I have solved the problem with your help.

Now I have another two question:

1)Can I download a s19 file with BDM and Codewarrior 2.10 ?And how I can download a s19 file to MPC5675K with your product ?

2)Is there any Bug with AA13pin and E20 pin of MPC5675K?

0 Kudos
Reply

937 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

1. Yes. Run this program:

c:\Program Files\Freescale\CW for MPC55xx and MPC56xx 2.10\pemicro\cw_progppcnexus.exe

2. I'm not aware of any issues. What's the problem?

Lukas

0 Kudos
Reply

937 Views
博张
Contributor I

Hi,lukas:

Thank you very much for your help.We have solved the problem with your help.Thank you.

0 Kudos
Reply