While researching interrupt logic on the MPC5748G processor, on page 611 in the document MPC5748GRM.pdf, Rev.4, bits in PRC_SEL in register INTC_PSRn are shown to be only 3 bits, but looking at source for examples it appears to be 4-bits and aligned differently. The example code that comes with the S32 Studio, V1.1 has the following configuration so some help here would be appreciated.
From pit.c in hello+pll+interrupt example.
INTC.PSR[226].B.PRC_SELN = 0x8; /* IRQ sent to Core 0 */
INTC.PSR[227].B.PRC_SELN = 0x4; /* IRQ sent to Core 1 */
INTC.PSR[228].B.PRC_SELN = 0x2; /* IRQ sent to Core 2 */
解決済! 解決策の投稿を見る。
priority select is 3 bits, but is up-aligned (if I may state it this way), in the MPC documentation "0" is MSB and "15" or "31" is LSB, so PRC_SEL is like it is defined also in the header files (it works this way, checked!):
union {
vuint16_t R;
struct {
vuint16_t PRC_SELN0:1;
vuint16_t PRC_SELN1:1;
vuint16_t PRC_SELN2:1;
vuint16_t :1;
vuint16_t :3;
vuint16_t SWTN:1;
vuint16_t :4;
vuint16_t PRIN:4;
} B;
} PSR[1024];
As you see, examples are also correct, they are using bits 0, 1 and 2 (0x8, 0x4, 0x2).
priority select is 3 bits, but is up-aligned (if I may state it this way), in the MPC documentation "0" is MSB and "15" or "31" is LSB, so PRC_SEL is like it is defined also in the header files (it works this way, checked!):
union {
vuint16_t R;
struct {
vuint16_t PRC_SELN0:1;
vuint16_t PRC_SELN1:1;
vuint16_t PRC_SELN2:1;
vuint16_t :1;
vuint16_t :3;
vuint16_t SWTN:1;
vuint16_t :4;
vuint16_t PRIN:4;
} B;
} PSR[1024];
As you see, examples are also correct, they are using bits 0, 1 and 2 (0x8, 0x4, 0x2).