I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

567 Views
yinlei
Contributor III

I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

Tags (3)
0 Kudos
1 Reply

459 Views
taokang
Contributor III

hello,

The tile 8 is best suitable for FFT processing.Because the TRAM/ORAM is accessed 8 slice at once.