How to use PKCS#12 in mpc5748G board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use PKCS#12 in mpc5748G board

779 Views
jiteshkamboj
Contributor I

Hi,

I am using the MPC5748G board. I have generated a signed certificate in PKCS#12 format(.p12) on my Windows PC. I want to use this certificate on the MPC5748G board. 

1. How this certificate can be flashed into the Board? i.e. Is there any tool to flash the certificate to the desired location or Something else need to be used 

2. How this certificate is used in the board. i.e. Is there any software library that can be used? or Something else.

3. PKCS#12 format include public and a private key, How this private and public can be fetched by embedded software when PKCS#12 format certificate is flashed on the board?

4. Do I required a security document to solve the above mention problem? which will be provided after signing the NDA with NXP.

0 Kudos
3 Replies

759 Views
akhileshkg
Contributor II

Hi Peter,

our main challenge is how to transfer/ flash the pkcs 12 file from our windows PC to board (NXP 5748G)! Something that Jitesh posted in question (1).

Could you help us on that?

Thanks,

0 Kudos

748 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I really have no experience here.

You want to program output file to micro? Is it compiler with supporting compiler for MPC5748G?

If yes, you can use any supported JTAG programmer for that.

Best regards,

Peter

0 Kudos

770 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

PCKS#12 is not supported by SPC5748G firmware.

Only PCKS#1.

Best regards,
Peter

 

 

0 Kudos