How to add leds to indicate the state of FCCU0 and FCCU1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add leds to indicate the state of FCCU0 and FCCU1

779 Views
AllanAn
NXP Employee
NXP Employee

PL see the picture below:

FCCU.PNG

what's the state of FCCU0 and FCCU1  ("0" or "1"),  when an error occurs ?

I want to add leds to indicate the state of FCCU0 and FCCU1, where can I add them?

if FCCU0 and FCCU1 have the ability to drive the LED(about 2mA) ?

Thank you for your answer !

0 Kudos
Reply
2 Replies

618 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if you use bi-stable protocol, then you could possibly use these signal for driving LEDs.

pastedImage_1.png

I would recommend to drive base of the transistor and put LED to the collector of the transistor. Of course, some resistors will be needed to use to set right working point.

Here I have found some article for inspiration:

Driving an LED using a Transistor 

Hope it helps

0 Kudos
Reply

618 Views
AllanAn
NXP Employee
NXP Employee

OK, thank you very much, David

BRs

0 Kudos
Reply