How to add leds to indicate the state of FCCU0 and FCCU1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add leds to indicate the state of FCCU0 and FCCU1

778 次查看
AllanAn
NXP Employee
NXP Employee

PL see the picture below:

FCCU.PNG

what's the state of FCCU0 and FCCU1  ("0" or "1"),  when an error occurs ?

I want to add leds to indicate the state of FCCU0 and FCCU1, where can I add them?

if FCCU0 and FCCU1 have the ability to drive the LED(about 2mA) ?

Thank you for your answer !

0 项奖励
回复
2 回复数

617 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if you use bi-stable protocol, then you could possibly use these signal for driving LEDs.

pastedImage_1.png

I would recommend to drive base of the transistor and put LED to the collector of the transistor. Of course, some resistors will be needed to use to set right working point.

Here I have found some article for inspiration:

Driving an LED using a Transistor 

Hope it helps

0 项奖励
回复

617 次查看
AllanAn
NXP Employee
NXP Employee

OK, thank you very much, David

BRs

0 项奖励
回复