Hello NXP community I m working on an automotive project. I m using MPC5603B,I m able to put the controller in STANDBY mode but it is not exiting STANDBY mode into DRUN mode ? How do I exit the Standby Mode ? Also how do i reduce the current consumption <

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello NXP community I m working on an automotive project. I m using MPC5603B,I m able to put the controller in STANDBY mode but it is not exiting STANDBY mode into DRUN mode ? How do I exit the Standby Mode ? Also how do i reduce the current consumption <

591 Views
abhayambekar
Contributor I

Hello NXP community I m working on an automotive project. I m using MPC5603B,I m able to put the controller in STANDBY mode but it is not exiting STANDBY mode into DRUN mode ? How do I exit the Standby Mode ? Also how do i reduce the current consumption <1mA ?

Labels (1)
0 Kudos
1 Reply

413 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Look at AN4240: http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4240.pdf .

The low power modes are discussed there and a guide to create lpm application is given there too.

BR, Petr

0 Kudos