I am trying to configure flexCan A, B, C and D modules. I have configured A and B modules and setup a number of the buffers to receive and transmit CAN frames. Flex CAN_A and CAN_B are fully functional. However, if I use the same code and functions with CAN_C and CAN_D base address it doesn't work. Does anyone know if there is anything else different other than the base addresses between CANA/B and CANC/D? Can also use an example code on how to set up flex can C and D.
Thank you
Hi,
CANC/D are on PBridge_A while CANA/B on PBridge_B. So check the PBridges setting.
BR, Petr