FlexCAN C and D modules for mpc5777c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCAN C and D modules for mpc5777c

585件の閲覧回数
amir_asemanpaye
Contributor I

I am trying to configure flexCan A, B, C and D modules. I have configured A and B modules and setup a number of the buffers to receive and transmit CAN frames. Flex CAN_A and CAN_B are fully functional. However, if I use the same code and functions with CAN_C and CAN_D base address it doesn't work. Does anyone know if there is anything else different other than the base addresses between CANA/B and CANC/D? Can also use an example code on how to set up flex can C and D.

Thank you 

0 件の賞賛
返信
1 返信

455件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

CANC/D are on PBridge_A while CANA/B on PBridge_B. So check the PBridges setting.

BR, Petr

0 件の賞賛
返信