Hello all,
I want to start testing my MPC5748G with some reference or example projects (can be baremetal without OS as well). If possible, I like to include and integrate several drivers in the future:
- CAN bus
- LIN bus
- FlexRay bus
- Ethernet port
- SPI port
Could you help me to find projects for that MCU or for similar ones?
Thanks,
kind regards,
Tobias
已解决! 转到解答。
You need AN4830, which contains all but FlexRay example. For FlexRay you'll have to use proprietary stack from AUTOSAR supplier or Vector (due to licensing issues).
Hello Aleksandar,
thank you very much. The examples are very helpful. But I am struggeling with the declaration of the function, since I can't find its definition:
__ghs_board_devices_init_AFTER_main(void);
Is that the actual name of it or will I substitute board_devices with its name?
Thanks,
regards,
Tobias
Hi Tobias,
__ghs_board_devices_init_AFTER_main is defined in
<zip file>\AN4830_rev1_SW\MPC5748G_rev<revision>_silicon\tgt\libboardinit\mpc5748g_rev1.ppc
Normally, compiler should find it, since demo projects contain and build
tgt\resources.gpj
which builds libboardinit.gpj, containing mentioned file.
BR,
Alex