Hello,
Sorry to trouble you.
My question is:
1. How to config the IVPR in Z7 cores?
I have config the IVPR in Z4 core(mtIVPR address), and works well. Can I use the same method to config the IVPR in Z7 cores(mtIVPR address, just the address is diffrent)
2. When a exception occur(eg. miss-align ) in Z7 core, exception handler function will not be called(Just notify the exception handler in Z7 core), am I right?
3. When I call the interrupt enable (asm(" wrteei 1")) in Z7 core, does it affect the Z4 core?
4. Can you tell me how to get the core ID in greenHills envirenment? I use "__MFSPR(286)" , but the return value is wrong.
Is there the documents describing the above knowledges?
Thanks very much?
已解决! 转到解答。
Hi,
1) For instance following way:
#IVPR = address base used with IVOR's
e_lis r5, __IVPR@h
e_or2i r5, __IVPR@l
mtIVPR r5
2) I am afraid I don’t understand this question at all. Could you clarify it?
3) No, the instruction affects the core executing this instruction.