Erasing NVSCI and NVPWD in shadow block for MPC5643L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Erasing NVSCI and NVPWD in shadow block for MPC5643L

Jump to solution
716 Views
YazenAlali
Contributor I

Hi,

When I use the Flash File To Target window in code warrior to erase the shadow block as below:

YazenAlali_0-1648825414145.png

NVSCI censorship memory and NVPWD0,NVPWD1 doesn't erase to al 0xFF's but they return back to their reset state defined in the reference manual as:
NVSCI=0x55AA55AA, NVPWD0=0xFEEDFACE, NVPWD1=0xCAFEBEEF

YazenAlali_1-1648825574170.pngYazenAlali_2-1648825590929.png

Is this normal for these memory registers as I know erasing means turning memory values back to 0xFF's? Do I expect the same behavior when running the shadow block erase from my application code?

Thanks,

0 Kudos
1 Solution
686 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

This is something I would not recommend to do as erasing of shadow flash followed by reset leads in permanent device lock-up.

If shadow flash is erased, it is needed to be immediately loaded by valid censorship configuration.

View solution in original post

0 Kudos
2 Replies
687 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

This is something I would not recommend to do as erasing of shadow flash followed by reset leads in permanent device lock-up.

If shadow flash is erased, it is needed to be immediately loaded by valid censorship configuration.

0 Kudos
676 Views
YazenAlali
Contributor I

Thank you for the reply

0 Kudos