Erase/Program Disturb Limits for MPC5777C Flash Memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Erase/Program Disturb Limits for MPC5777C Flash Memory

1,232 次查看
charukamboj
Contributor II

I have a query related to MPC5777C Controller - FLASH Memory.

The datasheet does mention about the Number of program/erase cycles per block & data retention.

But I want to confirm if there are any erase/program disturb limits also? Will they vary as per temperature ranges?

Note: Disturb limits for Flash : This is the limit to study the robustness of the data storage of the flash cells when the state of a nearby cell is being changed, either through erasing, programming or reading. A disturb failure means that the initial state of the cell has been changed to the opposite state as result of erasing, programming or reading.

0 项奖励
回复
1 回复

1,021 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

But I want to confirm if there are any erase/program disturb limits also? Will they vary as per temperature ranges?

There are no limits except Number of program/erase cycles per block & data retention in datasheet.

regards,
Peter

0 项奖励
回复