I am using DEVKIT-MPC5748G with DEVKIT-COMM & S32DS & example MPC5748G-FlexCAN_with_interrupts-S32DS_Z4_1
I want to use the Can Interfaces on the COMMs board, but cannot get the GPIO config right.
I have the "IO_Signal_Description_and_Input_multiplexing_tables.xls" but cannot understand it.
Can someone send me the config, to get the 4 CanPorts on the COMMs board working ?
Eg
in GPIO_Init()
// CAN_1 *** This Config Works for the RXCAN_A on the COMMs board ***
SIUL2.MSCR[42].B.SSS = 1; /* Pad PC10: Source signal is CAN1_TX */
SIUL2.MSCR[42].B.OBE = 1; /* Pad PC10: Output Buffer Enable */
SIUL2.MSCR[42].B.SRC = 3; /* Pad PC10: Maximum slew rate */
//
SIUL2.MSCR[43].B.IBE = 1; /* Pad PC11: Enable pad for input - CAN1_RXD */
SIUL2.IMCR[189].B.SSS = 3; /* CAN1_RXD: connected to pad PC11 */
// CAN_2 *** This Config FAILs for the RXCAN_B on the COMMs board ***
SIUL2.MSCR[64].B.SSS = 1; /* Pad PE01: Source signal is CAN2_TX */
SIUL2.MSCR[64].B.OBE = 1; /* Pad PE01: Output Buffer Enable */
SIUL2.MSCR[64].B.SRC = 3; /* Pad PE01: Maximum slew rate */
SIUL2.MSCR[65].B.IBE = 1; /* Pad PE00: Enable pad for input - CAN2_RXD */
SIUL2.IMCR[193].B.SSS = 1; /* CAN2_RXD: connected to pad PE00 */
Thank you.