Hi,
Regarding etpu. As I understand it, for MPC5636 the crank input should be connected to etpu channel 0.
I am now using mpc5777C and I downloaded the example AN4908SW for MPC5746R (closest match) where I see that the cam input is instead used for etpu channel 0.
/* Setup eTPU A inputs */
SIUL2.MSCR512_955[512-512].R = 9; // eTPU A ch0 = PH[11]
SIUL2.MSCR0_255[123].R = 0x008A0000; // PH[11] -> PH[11] - Cam
SIUL2.MSCR512_955[514-512].R = 9; // eTPU A ch2 = PH[13]
SIUL2.MSCR0_255[125].R = 0x008A0000; // PH[13] -> PH[13] - Crank
I am a little confused about this. Do you have any recommendation where to put the crank and cam input signal for mpc5777C?
Mathias
解決済! 解決策の投稿を見る。
The constraint is not an eTPU feature, it is a feature of the engine management microcode.
The CRANK input signal (section 4.1.2 of AN4907) has to be on either channels 0, 1, or 2, but if you decide to use 0 do some reading as to what "input signal connected to TCRCLK" implies but does not state.
On my project, using MPC5634M, I built a simulator with the cam and crank output generation code (TG) on channels 1 and 3 respectively, and these are jumpered to cam and crank inputs on channels 0 and 2 respectively.
The cam code doesn't care which pin it is associated with, and you can have more than one cam input. The constraint is on the crank signal. Stick to channels 1 or 2.
Non-authoritatively,
Andrei (from The Great White North)
The constraint is not an eTPU feature, it is a feature of the engine management microcode.
The CRANK input signal (section 4.1.2 of AN4907) has to be on either channels 0, 1, or 2, but if you decide to use 0 do some reading as to what "input signal connected to TCRCLK" implies but does not state.
On my project, using MPC5634M, I built a simulator with the cam and crank output generation code (TG) on channels 1 and 3 respectively, and these are jumpered to cam and crank inputs on channels 0 and 2 respectively.
The cam code doesn't care which pin it is associated with, and you can have more than one cam input. The constraint is on the crank signal. Stick to channels 1 or 2.
Non-authoritatively,
Andrei (from The Great White North)
Thanks a lot, much appreciated!