ESCI_A.SR.B.RDRF flag is not set on mpc5634xm uController

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ESCI_A.SR.B.RDRF flag is not set on mpc5634xm uController

1,510件の閲覧回数
andre_mocci
Contributor I

Hi everybody.

Actual severity of this issue is more than super critical!
I am developing a diagnostic application based on eSCI transmission; an external diagnostic tool will connect to the ECU using serial communication and standard KWP2000 protocol; K-Line uses eSCI peripheral to start, stop and handle communication with the ECU; unfortunately, tracing data through Lauterbach Trace32, I have seen that when I send an SCI frame (oscilloscope confirms that it arrives correctly to RXDA pin in the uController) the ESCI_A.SR.B.RDRF flag is not set (a break point in read/write access confirms it), so it is not possible for me to catch the ISR and to do next operations.
Why? Have you got any suggestions?

 

Thank you in advance

 

Andrea

ラベル(1)
タグ(1)
0 件の賞賛
2 返答(返信)

1,288件の閲覧回数
jonr
Contributor III

I use DMA to send/receive bytes from the eSCI port.

0 件の賞賛

1,288件の閲覧回数
andrea_mocci
Contributor II

Hi john...unfortunatly I am encoutering same problems using SCI to support LIN slave node. Do you have any example of DMA usage with SCI?

Thank you in advance

Andrea

0 件の賞賛