EQADC Calibration on MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EQADC Calibration on MPC5777C

ソリューションへジャンプ
866件の閲覧回数
berat24
Contributor III

Hello everyone,


There are two photos attached below. One of them is from an example whereas another is from a document about EQADC calibration.

In first photo, OCC was calculated by multiplying raw_res75 and GCC which was multiplyed with 16384 on the previous code line. However, in another photo, OCC was calculated without 16384. Which one is correct? Could you inform me?

Sincerely.

1.PNG2.PNG

0 件の賞賛
1 解決策
850件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Calculation are based on following appnote:

https://www.nxp.com/docs/en/application-note/AN2989.pdf

GCC is an unsigned 15-bit fixed point value with a single-bit integer portion and a 14-bit fractional
portion.

OCC is a signed 14-bit integer value.

 

16384 = 0x4000, this is due to conversion from float to fractional format

元の投稿で解決策を見る

0 件の賞賛
1 返信
851件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Calculation are based on following appnote:

https://www.nxp.com/docs/en/application-note/AN2989.pdf

GCC is an unsigned 15-bit fixed point value with a single-bit integer portion and a 14-bit fractional
portion.

OCC is a signed 14-bit integer value.

 

16384 = 0x4000, this is due to conversion from float to fractional format

0 件の賞賛