ECC injection on MPC5746C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECC injection on MPC5746C

1,213 Views
ddt_1793
Contributor II

Hi everyone,

I am developing ECC feature on MPC5744C and getting confusion when trying to create a ECC fake fault (ECC injection) for testing.

At here, davidtosenovjan‌ suggested that can inject via EIM but I couldn't found the same module in MPC5746C. My question is:

- Is there EIM module supported on MPC5746C chip?

- If EIM was not supported, Are there any alternative way to inject ECC on this chip?

Thanks,

Tung Dao.

Labels (1)
4 Replies

862 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I have just created example code based on approach I have already described in the link mentioned by you:

Example MPC5744P 1b+2b_RAM_ECC_error_injection GHS714 

This approach could be possible to use for RAM error injection on MPC5746C. Flash errors does not need to be injected as there are prepared faulty patterns in UTEST area. Error injection module is not present on MPC5746C device.

862 Views
ddt_1793
Contributor II

Thanks for the example.

As your code, Which address will getting corruption? Is it possible to change the corrupted address and where?

Thanks for you support.

Tung Dao.

0 Kudos

862 Views
木子李
Contributor II

Do you have IO_Signal_Description_and_Input_multiplexing_tables.xls about MPC5746C ?

0 Kudos

862 Views
ddt_1793
Contributor II

yes I have, I have "MPC5746C Reference Manual" which was attached "IO_Signal_Description_and_Input_multiplexing_tables.xls".

Which is information you want in that sheet?

0 Kudos