Does MPC5744 LINFlexd can use the TJA1021 Lin tranceiver?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does MPC5744 LINFlexd can use the TJA1021 Lin tranceiver?

390件の閲覧回数
ykp3036
Contributor I

Because TJA1021 is the UART to LIN, so can MPC5744 LINFlexd use the TJA1021 Lin tranceiver?Is LINFlexd diffenrent from UART-LIN in physical transmission ?

0 件の賞賛
返信
1 返信

371件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the LINFlexD module offers LIN mode, supports LIN protocol version 1.3, 2.0, and 2.1 and the TJA1021 is LIN transceiver, connection is normally possible using TXD and RXD pins. 

PetrS_0-1677487586450.png

The transmit data stream of the protocol controller at the transmit data input (TXD) is converted by the TJA1021 into a bus signal. The receiver detects the data stream at the LIN bus input pin and transfers it via pin RXD to the microcontroller.

BR, Petr

0 件の賞賛
返信