I am using MPC5676R micro, trying to transmit data from SPI A to SPI B. Data transfer between SPI channels are through DMA. But data transaction is not happening via DMA, PUSHR register is got getting updated. Loopback test between cross processor and cross channel is passed without DMA. Any suggestions. Any example code to prove DSPI transfer using DMA. Please do needful.
Hi Lukas,
I have progressed with the example, but now I have the performance issue with DMA. I am supposed to transfer 3746 bytes from Master DSPI A channel to Slave DSPI B Channel in multi transfer mode. But the data is TXFIFO is not been completely received by RXFIFO. If you have any proven code to transfer more than 2K bytes in multi transfer over DMA, it would be helpful. On a overview the Data transfer is shown below for your understanding,
Application --> DMA buffer(DMA) --> TXBUF(DMA)-->TXFIFO (DSPI_A) ===> DSPI_B(RXFIFO)(DMA) --> Application
Please do needful, as it is emergency to resolve the issue.
Hi,
I can't see any problem if you need to send more data. If you are able to transfer small block of data but not the larger one then I would try to decrease the SPI frequency to see if it is caused by some noise on SPI bus. Have you checked by oscilloscope if the data are sent by the master? Is it possible that it is caused by slave? This would require some extensive debugging...
Regards,
Lukas
One more observation, I have derived the register values from your code , but the able to see the data on TXFIFO and count is getting incremented on SPI A channel. But on SPI B channel no count value is seen and no data on POP register. Bit confused further where to observe and make SPI working. Please suggest.
Hi,
I get data from via DMA and put it on Spi A channel which acts as a master
and always transmits and SPI B channel acts as slave and always receives
data from tx fifo of channel A. Now I get data till tx fifo and count
getting updated and on rx side I don't see anything updated. Please share
your register configuration for spi A and B with DMA.
PFA configuration for reference. Please suggest.
Hi,
I do not understand from your description if there's a problem only with DMA or with the slave SPI module. Are you able to send/receive data from SPI B when not using DMA?
There's simple example for DSPI master/slave in AN2865:
http://www.nxp.com/files/32bit/doc/app_note/AN2865.pdf
http://www.nxp.com/webapp/sps/download/license.jsp?colCode=AN2865SW
It's not directly for MPC5676R but it could help...
Regards,
Lukas
Hi Lukas,
I have progressed with the example, but now I have the performance issue with DMA. I am supposed to transfer 3746 bytes from Master DSPI A channel to Slave DSPI B Channel in multi transfer mode. But the data is TXFIFO is not been completely received by RXFIFO. If you have any proven code to transfer more than 2K bytes in multi transfer over DMA, it would be helpful. On a overview the Data transfer is shown below for your understanding,
Application --> DMA buffer(DMA) --> TXBUF(DMA)-->TXFIFO (DSPI_A) ===> DSPI_B(RXFIFO)(DMA) --> Application
Please do needful, as it is emergency to resolve the issue.
Hi Lukas,
The screenshot I shared is the configuration done for SPI channel A and B.
Without DMA I am able to transfer from channel A to B. It would be helpful
if I get sample code for MPC5676R with SPI-DMA to directly test on my
target.
I am using 180 Mhz cpu clock with 40Mhz crystal, please suggest. My SPI
transfer is not happening and SPI is made to function as half duplex i. e.,
Spi A used to transmit and B used to receive alone. Please suggest
I need a quick help, for data transaction I using EDMA channel B 15 and for CRC checking Channel 47. Can you help me in configuring the necessary registers, earlier atleast I was able to see data in TXFIFO after updating the channel numbers in RSER, SERQR, ERQRL and ERQRH for channel 15 and 47 but unable to see data in DMA memory and TXFIFO. Can you help me in configuring correctly for DMA section. Please do needful