Dear Officer,
We have one DVKIT-MPC5744P REV E. and want to verify the CAN communication. We use PC/PCAN device to connect with CAN connector on DEVKIT board, and trying the FlexCAN_MPC5744P example code, but Neither configure (DEVKIT and LOOPBACK) options seems working. Can I check?
1. the CAN connector on DVKIT is connecting to CAN0 with PB0 and PB1?
2. What is configuration/changing to make this sample code to work with my setup: TX/RX CAN data from PC via PCAN to DEVKIT REV E CAN connector?
Thanks and best regards
He Wei
解決済! 解決策の投稿を見る。
Hi,
If referring to FLEXCAN_MPC5744P demo example available within S32DS, seems this will not work by default with DEVKIT rev.E board as was done for the previous one. I do not have this rev E board, only the older one, but as per the schematic (rev.E) :
- LINFlex_0 (PB2/PB3 pins) is connected to MK20 MCU, which serve as OpenSDA and virtual serial port
- FlexCAN_0 (PB0/PB1) is connected to SBC's CAN transceiver
So try to modify can.h to have
#define DEVKIT 0
This way you should see messages on terminal program. FlexCAN_0 stays in loopback mode, so nothing will be seen on CAN connector (P111).
To allow FlexCAN_0 communicate with other node, below modifications should be done too:
- within initCAN_0 comment line
CAN_0.CTRL1.B.LPB = 1; //Enable loopback mode
BR, Petr
Hi,
If referring to FLEXCAN_MPC5744P demo example available within S32DS, seems this will not work by default with DEVKIT rev.E board as was done for the previous one. I do not have this rev E board, only the older one, but as per the schematic (rev.E) :
- LINFlex_0 (PB2/PB3 pins) is connected to MK20 MCU, which serve as OpenSDA and virtual serial port
- FlexCAN_0 (PB0/PB1) is connected to SBC's CAN transceiver
So try to modify can.h to have
#define DEVKIT 0
This way you should see messages on terminal program. FlexCAN_0 stays in loopback mode, so nothing will be seen on CAN connector (P111).
To allow FlexCAN_0 communicate with other node, below modifications should be done too:
- within initCAN_0 comment line
CAN_0.CTRL1.B.LPB = 1; //Enable loopback mode
BR, Petr
Dear Petr,
Tks a lot
BR
He Wei