CodeWarrior 10.6 Erase Flash Config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 10.6 Erase Flash Config

1,153件の閲覧回数
jinjingyang
NXP Employee
NXP Employee

Dear Sir,

 

Customer is using CW10.6 to develop MPC5606B software.

By default, when we launch the debugger, it will erase all flash and program the elf into MCU.

Can we modify some configurations to make it erase only the specified area of flash and program elf file?

(For example, customer want to keep the bootloader area from 0x00000000~0x00010000 unchanged, and erase/program the flash area after 0x00010000.)

 

Regards,

Jason Yang

ラベル(1)
0 件の賞賛
1 返信

836件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Jason,

yes, there is a feature, which allows to keep some content of flash memory.

Open Debug configuration of your project (flash target) and click Edit

pastedImage_1.png

Choose Advanced Programming Options

pastedImage_2.png

Choose the memory range you do not want to erase during programming.

pastedImage_3.png

Hope it helps.

Regards,

Martin

0 件の賞賛