Clock frequency in MPC5777M-512DS board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock frequency in MPC5777M-512DS board

834 Views
alainfelici
Contributor I

Hello all, 

I am using an MPC5777M and the MPC5777M-512DS board. 

First of all, I wasn't not able to find MPC5777M-512DS documentation (jumper position and so on). In the MPC5777M EVB User Guide, the daughter card described is the MPC5777M_416DS. 

I have downloaded and run the ToggleStationery sample. I is running well, but the frequency of the flashing LED seems to be too slow: 1.5 second instead of 1.

As I wrote, I don't know was is the frequency of the XOSC reference. May be the jumpers are not in the rigth place.

Did someone as an idea?

Alain 

0 Kudos
5 Replies

591 Views
alainfelici
Contributor I

Hello all, 

I have found the problem. 

In the MPC5777M-PinToggleStationery sample, the PLL0 division is wrong. 

It is: MC_CGM.AC0_DC0.R = 0x80050000;    // PER_CLK : Enable aux clk 0 div by 4 … (75 MHz)

It is not a divide by 4 but by 6 and the result is not 75MHz but 50MHz. 

The good one should be : MC_CGM.AC0_DC0.R = 0x80030000; In this case we got a real 75MHz.

By the way, if someone can give me the code to get CLKOUT on the PF[8] or in the PV[0], I will be very happy. 

Thanks to all 

Alain

0 Kudos

591 Views
petervlna
NXP TechSupport
NXP TechSupport

Here you go:

    // Configure PF[8] as SYSCLK0
    // SIUL must be configured after mode transition!
    SIUL2.MSCR_IO[88].R = 0x02000000 | 0x01;  //PF[8] - ODC_PUSH_PULL and SSS_PF8_SYSCLK0

and:

    //Clk Out
    MC_CGM.AC6_SC.R = 0x02000000;        //Enable PLL0 - clkout0 //MC_CGM_AC6_SC
    MC_CGM.AC6_DC0.B.DE = 1;            //Enable divider for SYSCLK0
    MC_CGM.AC6_DC0.B.DIV = 0x13;        //Set divider for SYSCLK0 to 20

Peter

0 Kudos

591 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Jumper settings are described in chapter 3. Configuration—Motherboard.

http://cache.nxp.com/assets/documents/data/en/user-guides/MPC5777MEVBUG.pdf?fsrch=1&sr=1&pageNum=1 

Did you measured your clocks, and LED by scope to be sure?

First, measure CLKOUT pin to get information about system clock used, then calculate LED loop delay from system clock.

Peter

0 Kudos

591 Views
alainfelici
Contributor I

Hello Peter, 

Unfortunatelly, Jumpers for the 512DS daughter board are not described in this document (only for 416DS). I was not able to find documents for 512DS.

I don't know how to output CLKOUT.

My clock setting is the folowing:

// Set PLL0 to 300 MHz with 40MHz XOSC reference
// PREDIV = 1, MFD = 15, RFDPHI = 2, RFDPHI1 = 8
PLLDIG.PLL0DV.R = 0x4002100F;

MC_CGM.AC0_DC0.R = 0x80050000; // PER_CLK : Enable aux clk 0 div by 4 … (75 MHz)

PIT_0.TIMER[0].LDVAL.R = 75000-1; // setup timer 0 for 1msec period

With this configuration, the  LED GPIO output should change every 1ms. I can see a switch every 1.5 ms.

So, If I assure that my configuration is good, the problem can come from the jumper (I don't have the external OSC enabled) or the external clock don't have the good frequency.

Thanks for your help .

Alain  

0 Kudos

591 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Here is the part of EVB schematic for 512DS:

pastedImage_1.png

Measure system frequency on CLKOUT pin to be sure which is your actual system clock. It is PF[8].

pastedImage_2.png

Then you can calculate your LED loop time.

Peter

0 Kudos