Can the ECC checks be disabled on the MPC5777M?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can the ECC checks be disabled on the MPC5777M?

485件の閲覧回数
drgareth1978
Contributor I

We are getting a processor reset because of a double bit error on the flash originating from the ECC checks and would like to disable the checks and rely on the check sum to test the integrity of flash.

0 件の賞賛
返信
1 返信

433件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, ECC mechanism cannot be disabled.

The only exception is reporting of ECC events on data flash where ECC event reporting is suppressed, single-bit and multi-bit ECC errors are not reported (either to the core or to MEMU module). On multi-bit ECC event, the corrupted read data is replaced with a fixed, ECC-clean illegal opcode value of 0x1555_1555.

Single-bit ECC events on code flash accesses are automatically corrected and reported to the MEMU (if enabled). On multi-bit ECC event, core responds with bus error (IVOR1 exception) and an error is reported to MEMU module.

0 件の賞賛
返信