My PC's OS is windows 10. I installed tresos v24.0.0 tool.but it can't be loading when i open the tresos_gui.exe , with always stay in loading view.
And the window task manager shows his task"Java(TM) Platform SE binary" status is no response. when i closed the loading view,it show me the information like this(jdk-8u92-windows-i586 and jre-6u45-windows-i586 have been installed).
But Tresos v16.0.0 can loading his workspace normal.
Compared with tresos v16 and v24 's task status.
I have try to reinstall the tresos24 ,but the question can not be solved.
Thanks for your help.
解決済! 解決策の投稿を見る。
Hi,
Seems like there is an insufficient memory situation. You can try by increase maximum memory start of EB Tresos, by editing in tresos_gui.ini: -Xms256m => -Xms512m to see if the situation can be resolved. If it's not working, then maybe contacting Elektrobit support team directly is a better idea (https://www.elektrobit.com/support/)
Hello @flatcloud1 ,
Access has granted. Please check in your SW licensing account -> EB tresos tool.
Best Regards,
Nam
Hello peter.jonsson@qrtech.se, everyone
In case that your request for the hot-fix has been processed, please check in your SW licensing and support >> Automotive SW - Elektrobit Tresos Studio >> Tresos Studio [Version, for instance 24.0.1], then download the hot-fix in zip. You guys can refer to the below snapshot.
Best Regards,
Nam
Hello Nam,
Sorry, but cannot find version 24.0.1.
Hello Nam,
For 23, does V23 also have a hot fix?
BR
Hello @_Hao_,
Yes, hot-fix for V23 is available. Let me ask the team to check it and grant access for you.
Best Regards,
Nam
@riglesias2021, please follow to below instruction to download the hot-fix
"In case that your request for the hot-fix has been processed, please check in your SW licensing and support >> Automotive SW - Elektrobit Tresos Studio >> Tresos Studio [Version, for instance 24.0.1], then download the hot-fix in zip. You guys can refer to the below snapshot.
"
Hi, i did a clean install of tresos 24.0, installed the hotfix ( just replaced plugins folder and overwrite all the files ), but it seems my tresos wont start
Please try to also update the EB license administrator to 1.4.0 version if possible. If it doesn't help, then please contact to Elektrobit for further support.
Hi,
I am facing the same issue with EB Tresos Studio Version 24.0.1
Can you please provide the hotfix ?
Mail Id: bydong@iflytek.com
Thanks
Hi,
I am facing the same issue with EB Tresos Studio Version 24
I have tried the suggestions above in this thread without success.
Can you please provide the hotfix ?
Mail Id: swapnil.misal@tcs.com
Thanks
Access granted. Please check your SW licensing and support.
Many thanks,
Nam
Hi,
I am facing the same issue with EB Tresos Studio Version 24.0.1, 25.1.1, 26.0.0
Can you please provide the hotfix ?
Mail Id: kexin.liu@nxp.com
Thanks
Hi,
I have the same issue with EB Tresos Studio Version 24
I have tried the suggestions above in this thread without success.
Can you please make the hotfix available for me?
My email: peter.jonsson@qrtech.se
Like others have reported, it was working perfectly and then suddenly it stopped working for some strange reason.
Thanks and Best regards
Access granted. Please check your SW licensing and support.
Many thanks,
Nam
Thank you, but I cannot find that I have any new files to download.
Could you provide more information on how to find it, or send by other means?
Best Regards,
Peter
Hello luciano.curti@silicon-gears.com,
Your request has been completed. Could you check in your Software Licensing support to see whether the fix is available?
Nam
Hi,
I have the same issue after installing EB Tresos Studio Version 24.0.1 and EB Client License Admin 1.3.0.
Is there a HF available for this version of Tresos as well?
I have already tried out with EB Client License Admin 1.2.4 and all the methods mentioned above without any success.
My NXP account would be benno.voggenreiter@esg.de.
Thanks and Best regards
Hello benno.voggenreiter@esg.de,
Yes, there's a hot-fix for EB 24.0. I will ask marketing team to allow you to download it and let you know once the request is finished.
Thanks,
Nam