CAN FEC Ethernet Module be tested with MPC5777c 516DS standalone daughter board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN FEC Ethernet Module be tested with MPC5777c 516DS standalone daughter board?

443件の閲覧回数
vignesh_v
Contributor III

I'm trying to implement the ethernet module (FEC) using MPC5777c 516DS . we are purchasing daughterboard only standalone.CAN FEC Module be tested with standalone (only daughterboard)?

I'm choosing RMII mode I'm referring the example code from AN4577 and the MPC5777M FEC example:

One More Query is it possible to do a TFTP module implementation without lwip or FNET stack? if soa ref link or eample would be appreciated..

Thanks In Advance

ラベル(1)
タグ(2)
0 件の賞賛
1 返信

372件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

1) CAN FEC Module be tested with standalone (only daughterboard)?

Unfortunately no, because Ethernet PHY is not presented in Daughter card, also, there is no connector available. I recommend you to buy MPC57xx Motherboard too.

2) One More Query is it possible to do a TFTP module implementation without lwip or FNET stack?

Theoretically it is possible, but you must implement Layer 3 and Layer 4 protocols on your own. Because TFTP is Layer 7 application protocol, IP and UDP must be available too. This is what FNET or LwIP implements by default.

Regards,

Martin

0 件の賞賛