Hello,
This is a continuation of this thread , the TX/RX for CAN-FD frame of 8 bytes works fine, i want to configure the module tu support 64bytes. the changes made so far are :
FDCTR
Increase message buffer to support 64 bytes
MB0 and MB1 seems to have the correctly lenght in the register view :
No interrupppt is triggered once i send a CAN frame from canoe. i think other configuration could be needed , below is the code for the config :
ErrorCode FlexCANDevice::init()
{
/* enable the FlexCAN module, reset and freeze */
fpDevice->MCR.R = (0
| CAN_MCR_FRZ /* enabled to enter Freeze mode */
| CAN_MCR_HALT /* enter freeze mode if FRZ bit is set */
//| CAN_MCR_SOFTRST /* soft reset */
//| CAN_MCR_SRXDIS /* self reception enable */
| CAN_MCR_BCC /* individual Rx masking and queue */
| 0x0000003F);
/* double check that we are actually in freeze mode */
while(0 == fpDevice->MCR.B.FRZACK) {};
while(0 == fpDevice->MCR.B.NOTRDY) {};
fpDevice->MCR.R = (0
| CAN_MCR_FRZ /* enabled to enter Freeze mode */
| CAN_MCR_HALT /* enter freeze mode if FRZ bit is set */
| CAN_MCR_SRXDIS /* self reception disabled */
| CAN_MCR_BCC /* individual Rx masking and queue */
| CAN_MCR_AEN /* Safe Tx abort enable */
| CAN_MCR_FDEN /* CAN FD enabled */
| 0x0000003F); /* enable 64 MBs */
// Set CAN Bit Timing Register (CAN_CBT. P-1747)
fpDevice->CBT.B.BTF = 1; // Enable extended bit time definitions
fpDevice->CBT.B.EPRESDIV = fConfig.bitrate_cbt.presDiv;
fpDevice->CBT.B.ERJW = fConfig.bitrate_cbt.rjw;
fpDevice->CBT.B.EPROPSEG = fConfig.bitrate_cbt.propSeg;
fpDevice->CBT.B.EPSEG1 = fConfig.bitrate_cbt.pSeg1;
fpDevice->CBT.B.EPSEG2 = fConfig.bitrate_cbt.pSeg2;
// Set CAN FD Bit Timing register (CAN_FDCBT. P-1768)
fpDevice->FDCBT.B.FPRESDIV = fConfig.bitrate.presDiv;
fpDevice->FDCBT.B.FRJW = fConfig.bitrate.rjw;
fpDevice->FDCBT.B.FPROPSEG = fConfig.bitrate.propSeg;
fpDevice->FDCBT.B.FPSEG1 = fConfig.bitrate.pSeg1;
fpDevice->FDCBT.B.FPSEG2 = fConfig.bitrate.pSeg2;
// Set CAN FD Control register (CAN_FDCTRL .P-1766)
fpDevice->FDCTRL.R = 0;
fpDevice->FDCTRL.B.FDRATE = 1; // bit rate switching enable
fpDevice->FDCTRL.B.TDCEN = 0;
//fpDevice->FDCTRL.B.TDCOFF = 32;
fpDevice->FDCTRL.B.MBDSR0 = fConfig.payload;
// Enable CAN ISO
fpDevice->CTRL2.B.ISOCANFDEN = 1;
// Setup message buffers
fRxInterruptMask = 0;
uint32_t mask = 1;
// Setup MB0 for sending
setupMessageBuffer(0, CANTxBuffer::CODE_INACTIVE, false);
// Setup MB1 for receiving
setupMessageBuffer(1, CANRxBuffer::CODE_EMPTY, false);
fRxInterruptMask |= mask;
mask <<= 1;
return CAN_ERR_OK;
}
void setupMessageBuffer(uint8_t bufIdx, uint8_t code, bool extended)
{
fpDevice->MB[bufIdx].CS.R = 0;
fpDevice->MB[bufIdx].CS.B.IDE = extended ? 1 : 0;
fpDevice->MB[bufIdx].CS.B.CODE = code;
fpDevice->MB[bufIdx].ID.R = 0;
for (int i = 0; i < 16; i++) {
fpDevice->MB[bufIdx].DATA.W[i] = 0;
}
fpDevice->RXIMR[bufIdx].R = 0;
}
Thank you.
Best regards.
解決済! 解決策の投稿を見る。
Hi,
yes, you have to, if want to use this structure.
You shared below
debugger shows MBs in right manner for 64byte payload but your init is wrong. Empty CODE for RX MB is on wrong offset.
BR, Petr
Hi,
be sure you are using right offset for MBs for higher payload setting. From the last picture it is evident you have still offset for 8byte payload setting. See chapter 73.6.5 FlexCAN message buffer memory map for more info
BR, Petr
Hi @PetrS
Thanks for the hint. offset is corrected now
but i could not receive interrupt when sending FD fram with 64byte payload , it works only with 8 bytes?
this is the register view :
Thank you.
Hi,
show repaired MB area, and specify what is send from CAN tool. Do you see any error detected there?
BR, Petr
Hello @PetrS
No the tool does not report any error, the data inside the frame is :
shouldn't we modify also the message buffer initialisation since we use 32-64 bytes ?
Best regards.
Hi,
yes, you have to, if want to use this structure.
You shared below
debugger shows MBs in right manner for 64byte payload but your init is wrong. Empty CODE for RX MB is on wrong offset.
BR, Petr
Hello @PetrS ,
Yes you are right, the address Offfset for the MB is wrong.
i could not find/oversee in datasheet where i can set the address offset for each MB ? i could only set the
Hi,
I already mentioned it in previous reply.
BR, Petr