Bootload from Ethernet on MPC5748G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootload from Ethernet on MPC5748G

1,451件の閲覧回数
arribaconsultin
Contributor I

Hello,

I'm looking to create a bootloader for the MPC5748G via Ethernet connection and was curious what previous development has been done with respect to this, if any, and see if anyone has resources that can point me towards the best path to achieve this.

The goal is to be able to push firmware to this board via ethernet and keep the device tucked away without needing to access it.

Whats the best way for me to go forward with this?

#MPC5748G #Bootload #Ethernet

Thanks!

ラベル(1)
タグ(3)
0 件の賞賛
3 返答(返信)

1,170件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

There’s serial bootloader for MPC5748G:
https://www.nxp.com/docs/en/application-note/AN5319.pdf
https://www.nxp.com/docs/en/application-note-software/AN5319SW.zip

Ethernet driver can be found in SDK in S32 Design Studio IDE:
https://www.nxp.com/support/developer-resources/run-time-software/s32-design-studio-ide/s32-design-s...

Hope this is a nice start point.

Regards,

Lukas

0 件の賞賛

1,170件の閲覧回数
bhavesh
Contributor II

Hi Lucas,

The bootloader you created looks interesting. I wanted to use the Zip that you pointed above with the S32 studio for MPC5748G. Is there a way t do that ? Or even if you can help me understand the structure of the code like where can I make the project if i were to edit it to make it work on CAN/LIN instead of UART.

Thank you.

Regards,

Bhavesh A. Rathod,

Member Of technical staff,

Gunakar Pvt. Ltd.

0 件の賞賛

1,170件の閲覧回数
1642280511
Contributor I

Hello, I am developing a can-based bootloader. May I ask if you can share your bootloader code for my reference? Thank you very much.

0 件の賞賛