Bit is reserved,Value must remain 1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bit is reserved,Value must remain 1

493件の閲覧回数
frank747
Contributor II

Hi all:

"Bit is reserved,and must not be writeen or cleared,Value must remain 1."

If the bit with the above description is changed to 0 by the software, what effect might it have?

MPC5125RM.pdf 5.3.1.2 Figure 5-7

タグ(1)
0 件の賞賛
1 返信

486件の閲覧回数
Pavel
NXP Employee
NXP Employee

Usually incorrect setting reserved bits can produce unpredictable behavior. Often these bits are used for different testing on the factory.

0 件の賞賛