MPC5xxx Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5xxx Knowledge Base

Labels
  • General 164
  • test 7

Discussions

Sort by:
IDE: CodeWarrior 10.6 mcu:MPC5606B Conversion Mode:Scan Channel: ADC1, 1\2\3\13\14 End of Chain Conversion interrupt enable; QQ:511437685
View full article
******************************************************************************** * Detailed Description: * * LINFlex UART TXFIFO transmit using DMA * LINFlex UART mode with FIFO receive using DMA * * * EVB connection: * *   Route LINFlexD_0 TXD/RXD (PB2/PB3) signals to the main board RS-232 transceiver *   Daughtercard: *   J17.11–12 ON  .. Connect LINFlexD_0 TXD (PB2) to main board. *   J17.8–9 ON .. Connect LINFlexD_0 RXD (PB3) to main board. * *   Motherboard *   J14 - SCI_RX ON *   J13 - SCI_TX ON *   J25 - SCI_PWR ON * * See results on PC terminal (baudrate 19200, Data bits 8, Stop bits 1, Parity none). * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  internal_FLASH (debug mode, release mode without debugging information) * Fsys:     200 MHz PLL with 40 MHz crystal reference * Terminal: 19200, 8N1, None ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * This example shows how to configure Wake up unit and CAN sampler. * Once the device is woken up from STOP mode by falling edge on CAN0RX pin, * the CAN sampler starts to sample this pin in given period. * FlexCAN module is not initialized and used in this example because the CAN * sampler is independent of FlexCAN. * ------------------------------------------------------------------------------ * Test HW:  XPC56xxMB2 + XPC560B 176LQFP, PPC5607B * Target :  internal_FLASH, RAM * Fsys:     64 MHz PLL * ********************************************************************************
View full article
Hardware:TRK-MPC560XB, IDE:codewarrior 10.6; External Crystal Oscillator: 8M System Core Frequency: 64MHz FlexCAN Baute rate: 250bps BUF[1] Interrupt, Bus Off Interrupt, Err Interrupt enable;   QQ:511437685
View full article