Example XPC564AKIT324S External SRAM test CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example XPC564AKIT324S External SRAM test CW210

Example XPC564AKIT324S External SRAM test CW210

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt, second LED by software

* loop, initializes and display notice via UART terminal and then terminal ECHO.

* The example configures the device for maximum performance (OPTIMIZATIONS_ON).

* IT INITIALIZES EBI FOR EXTERNAL SRAM CONNECTED TO XPC564AKIT324S AND TEST IT.

*

* ------------------------------------------------------------------------------

* Test HW:        XPC564AKIT324S

* MCU:            SPC5644AMVZ1 0M14X QAK1235G

* Fsys:           150/132/120/12 MHz

* Debugger:       Lauterbach Trace32

* Target:         RAM, internal_FLASH

* Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A

* EVB connection: default

*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎07-07-2014 12:21 AM
更新人: