Example MPC5777M PIT ISR GHS614

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5777M PIT ISR GHS614

Example MPC5777M PIT ISR GHS614

********************************************************************************

* Detailed Description:

*

* PIT channel 0 is used to generate 1sec interrupt where PA0 pin is toggled.

*

* ------------------------------------------------------------------------------

* Test HW:  MPC5777M, MPC57xx Motherboard + MPC5777M_512DS minimodule

* Maskset:  0N78H

* Target :  RAM, internal_FLASH

* Fsys:     600 MHz PLL1 with 40 MHz crystal reference

*               core2 at 200MHz generated from PPL1

* Terminal: None

********************************************************************************

Labels (1)
Attachments
No ratings
Version history
Last update:
‎02-11-2016 05:01 AM
Updated by: