********************************************************************************
* Detailed Description:
* Application performs basic initialization, setup PLL to maximum allowed freq.,
* initializes interrupts. STM_0 channel 0 is initialized to generate 100ms
* periodic interrupt. Notice that STM is free running up counter, so it's
* necessary to add calculated value to compare register each time in ISR handler.
*
* Test HW: X-MPC5744PE257DC, MPC57xx motherboard
* MCU: SPC5744PGMMM9 1N15P
* Fsys: 200 MHz
* Debugger: Lauterbach Trace32
* PeMicro USB-ML-PPCNEXUS
* Target: internal_FLASH (debug mode, release mode)
* EVB connection: User LED 1 connected to A0 (P8.0),
*
********************************************************************************