Example MPC5646C PinToggleStationery CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5646C PinToggleStationery CW210

Example MPC5646C PinToggleStationery CW210

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed freq.,

* initializes interrupts, blinking one LED by interrupt, second LED by software

* loop, third LED by second core, initializes and display notice via UART

* terminal and then terminal ECHO.

*

* ------------------------------------------------------------------------------

* Test HW:  XPC56xxMB2 + XPC564xB/C, PPC5646C 0M87Y silicon

* Target :  internal_FLASH, RAM

* Fsys:     120 MHz PLL0

* Debugger: Lauterbach Trace32. script for internal_FALSH run_from_flash.cmm

*                               script for RAM: run_from_ram_vle.cmm

*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎06-10-2016 01:20 AM
更新人: