Example MPC5604P FlexPWM Initialization on TRK board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5604P FlexPWM Initialization on TRK board

Example MPC5604P FlexPWM Initialization on TRK board

This simple example shows usage of the FlexPWM module on the TRK board.

If a PWM output is connected to the LED you can see its dimming.

 

Regards,

Petr

 

********************************************************************************

* Detailed Description:

*

* This example shows usage of FlexPWM module.

* The Submodule0 is set to generate independent PWMA and PWMB signals and vary

* its duty cycles. The PWMX is also enabled as output and is set for fixed 50%

* duty.

*  

* You can remove LED_EN jumpers and connect FlexPWM A an B outputs to LEDs to see

* its dimming.

*

* ------------------------------------------------------------------------------

* Test HW: TRK-MPC5604P

* Maskset:  0M36W

* Target : internal_RAM

* Terminal: no

* Fsys:     64 MHz with 8 MHz XOSC reference

* Debugger: IDCPPCNEXUS

*

* TRK board connection:

*

* P4.10 - D[9]  .. FlexPWM X[0] output

* P1.11 - A[10] .. FlexPWM B[0] output

* P1.12 - A[11] .. FlexPWM A[0] output

*

*

  ********************************************************************************

标签 (1)
附件
评论


Hi

100% 有帮助 (1/1)
版本历史
最后更新:
‎02-27-2014 12:26 AM
更新人: